Technical FAQs

Ask a Question

Do we make a three pole, 3 phase surge protector in a breaker style for use in a 3 phase QO panel ?

Issue:
Do we make a three pole, 3 phase surge protector in a breaker style for use in a 3 phase QO panel ? 

Product Line:
Surge Protection.

Environment:
Products sold in the United States.

Cause:
Product Availability.

Resolution:
Consider using 2 QO2175SB, one on either side of the panel . This combination wil provide 22k of protection on the A phase and the C phase and 44k on the B phase


CTA-ID : 2061209
Was this helpful?
What can we do to improve the information ?