Technical FAQs

Ask a Question

On an ATV312......M3X series drive, 200-240V input: At what voltage on the DC bus does the braking transistor turn on and conduct power through the braking resistor?

The braking transistor will turn on when the DC bus voltage reaches 379VDC.

CTA-ID : 2061129
Was this helpful?
What can we do to improve the information ?