Technical FAQs

Ask a Question

ATV61HC13N4 and ATV71HC11N4: What are the replacement cooling fans part numbers?

VZ3V1212 is a heatsink fan/blower .
VZ3V1214 is an internal 80mm x 80mm circulating fan powered with 24Vdc.

Note: If you replace the VZ3V1212 heat sink fan you will also need to replace the Fan control pwb part number VX5A1400.

CTA-ID : 2061260
Was this helpful?
What can we do to improve the information ?