Technical FAQs

Ask a Question

What is the cross to Powerpact for an ME36800LSG?

The cross is PJA36080U44A.  If the application is 3p4w (including a neutral), neutral CT S33576 is also required.


CTA-ID : 2061244
Was this helpful?
What can we do to improve the information ?