Technical FAQs

Ask a Question

What is a QO154L225PG?

Issue:

What is a QO154L225PG?

Product Line:

PTFDS - FD Enclosure Systems

Environment:

QO load centers sold and supported in the USA.

Cause:

Definition of the new catalog number QO154L225PG.

Resolution:

This is a new style of QO Load Center, referred to as ``PoN`` (Plug on Neutral), that has a specially designed branch neutral assembly that will accept new style QO CAFI ``PoN`` circuit breakers. The neutral connection from the QO ``PoN`` CAFI circuit breaker to the QO ``PoN`` load center branch neutral bar assembly is made automatically when the QO CAFI ``PoN`` breaker is installed onto the QO ``PoN`` load center bussing. The traditional method of connection was via a ``pigtail`` conductor on the CAFI breaker terminated into the load center branch neutral bar assembly.




CTA-ID : 2061201

Was this helpful?
What can we do to improve the information ?