Technical FAQs

Ask a Question

NQMB2Q Closing Plate

Issue:
What is the part number for the closing plate for a NQMB2Q?

Product Line:
NQ panelboards and accessories sold and supported in the USA.

Environment:
Maintenance

Cause:
Removal of the main breaker in an NQ panelboard will require a closing plate.

Resolution:
There is no closing plate available for this.  Suggest a local sheet metal fabricator make something to cover the opening.





CTA-ID : 2056186
Was this helpful?
What can we do to improve the information ?