Technical FAQs

Ask a Question

Are Series Rating available for QO Main Lug Only, 1 Phase load centers when using std QO 10,000 AIR branches ?

Issue:
Are Series Rating available for QO Main Lug Only, 1 Phase load centers when using std QO 10,000 AIR branches ?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
QO load centers sold and supported in the USA. 

Cause:
Determination of series ratings on QO load centers with variable branches and mains.

Resolution:
Series Ratings for current design Series S01 and S02 (Convertible Mains), 125 - 225 ampere, Main Lug Only, 1 Phase QO load centers include:
100,000 AIR with remote 100-200 ampere, 300Vac Class T fuses, or QJ 225A max breakers
65,000 AIR with remote QG 225a max main breaker
42,000 AIR with remote QOH main breaker
25,000 AIR with remove QD 225A max breakers
22,000 AIR with remote QO-VH or QOM-VH breakers.
The Main Lugs may be converted to a QOM-VH Main Breaker, providing a 22,000 AIR rating with Integral Main.
NOTE: for specific details on a particular load center, check the labeling prior to installation.





CTA-ID : 2061153
Was this helpful?
What can we do to improve the information ?