Technical FAQs

Ask a Question

What does PoN, or PON, stand for?

Issue:
What does PoN or PON stand for?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
QO load centers and circuit breakers sold and supported in the USA.

Cause:
Definition of PoN or PON.

Resolution:
It is an acronym for Plug-On Neutral. The term is used to describe the Plug-On Neutral of QO-PCAFI and QO-VHPCAFI circuit breaker and the associated QO PoN Load Centers that they can be used with.





CTA-ID : 2061212
Was this helpful?
What can we do to improve the information ?