Technical FAQs

Ask a Question

Can standard QO full size circuit breakers be used in the QO Plug-On Neutral Load Center?

Issue:
Application

Product Line:
QO Load Center

Cause:
Application of QO load centers and breakers

Resolution:
Yes, standard full size QO breakers, including ``pigtail`` GFCI, AFI and CAFI, can be used in the QO Plug-On Neutral Load Centers. However, the QO Plug-On Neutral Load Centers are not designed to accept QOT or QO tandem breakers.
 
 


CTA-ID : 2061213
Was this helpful?
What can we do to improve the information ?