Technical FAQs

Ask a Question

With the introduction of QO Plug-On Neutral Load Centers and Plug-On Neutral CAFI breakers, are standard QO Load Centers and CAFI breakers being obsoleted?

Issue:
With the introduction of QO Plug-On (PoN) neutral load centers and plug-on neutral CAFI breakers, are standard QO load centers and CAFI breakers being obsoleted?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
QO load centers and circuit breakers sold and supported in the USA.

Cause:
With the introduction of the new plug on neutral QO load centers and circuit breakers, the question will come up if the standard QO load centers and CAFI circuit breakers will be obsoleted and replaced.

Resolution:
No, there are no plans for obsolescence of the standard QO Load Centers, nor CAFI breakers, due to the launch of the QO Plug-On Neutral Load Centers and Plug-On Neutral CAFI breakers.

 

 

 

 

 




CTA-ID : 2061214

Was this helpful?
What can we do to improve the information ?