Technical FAQs

Ask a Question

Can the MHC74VS be replaced by the NC74VS?

Issue:
Can the MHC**VS vented trim for an NQOD panel  be replaced by the NC**VS vented trim used on the NQ panelboard? 

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboards sold and supported in the USA. 

Cause:
Interchangeability of the MHC**VS and the NC**VS.

Resolution
No .They are not interchangeable.




CTA-ID : 2057610
Was this helpful?
What can we do to improve the information ?