Technical FAQs

Ask a Question

What are the repair parts for the HU361A, series F6? (may be shown as F06)

Issue:
Repair Parts

Product Line:
HD SS 

Cause:
Maintenance

Resolution:
The replacement parts for the HU361A, series F6 (F06) are as follows. No other parts are available.

Line Base Assembly -40566-426-50 (requires one per switch. Arc suppressor assembly not included)
Line base mounting screw - 40205-160-01 (3-required)
Arc Suppressor Assembly - 40566-694-51 (requires one per switch)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Standard Lug Assembly - 40251-016-52 (requires 6 per switch) and Lug Mounting Nuts - 40205-154-01(requires one per lug)
Copper Lug kit(NOT STANDARD) - CL0306F (includes 6 lugs)
Switch Mechanism - 40566-107-50
Switch Mechanism Gasket - 40566-656-01 (one required)
Handle Assembly - 40566-841-50K
Handle Gasket - 40566-031-01 (one required)
Lockplate - 40566-376-01
Lockplate mounting screws - 22999-405-62 (2 required)




CTA-ID : 2061134
Was this helpful?
What can we do to improve the information ?