Technical FAQs

Ask a Question

What are the mounting hole dimensions for a XVLA`s?

8mm  for the XVLA1`s and XVLA2`s with a thread of M8 X .5 and 12mm for the XVAL3`s with a thread of M12 X 1.

CTA-ID : 2061095
Was this helpful?
What can we do to improve the information ?