Technical FAQs

Ask a Question

What is the difference between the 9036DG and the 9036GG?

The 9036 DG  is a lighter duty device.   Only the 9036GG is rated for 460V single phase,  has higher horsepower ratings at 460V 3 phase, and higher DC horspower ratings.


CTA-ID : 2061019
Was this helpful?
What can we do to improve the information ?