Technical FAQs

Ask a Question

What is the maximum ampere branch breaker that can be used on the 8space interior of the QU816D400CL?

On the 8-space interior a 200 amp branch breaker can be used as long as the installer doesn`t overload the mains rating for the device.



CTA-ID : 2060916
Was this helpful?
What can we do to improve the information ?