Technical FAQs

Ask a Question

NQALV1 Lug Kit

Issue:
What is included with main crimp lug kit NQALV1?

Product Line:
NQ panelboards and accessories sold and supported in the USA.

Environment:
NQ panelboard crimp lug kit.

Cause:
Determination of kit content.

Resolution:
Three main crimp lugs, one neutral crimp lug, three crimp lug pads, three keps nuts, one 1/4-20 x 9/16`` tapping screw, six 1/4-20 x 7/8`` tapping screws, two lug barriers.


 
Was this helpful?
What can we do to improve the information ?