Technical FAQs

Ask a Question

What is the maximum ampere rating for the QO2L30TTS?

Issue:
Application

Product Line:
QO LC

Cause:
Clarification of ampere rating

Resolution:
The maximum ampere rating for the QO2L20TTS is 30 amperes maximum.


CTA-ID : 2060981
Was this helpful?
What can we do to improve the information ?