Technical FAQs

Ask a Question

What does a H101 mean on a 9001KR12UH101?

The H* codes are suffixes added to the operator part number so that contact blocks are installed in specific sequences to perform specific operations. The H101 means a 9001KA2 contact block will be mounted in positions 1, 2, 3, 4, 5 and 6 of the push button.
Was this helpful?
What can we do to improve the information ?