Technical FAQs

Ask a Question

How does the new spring technology work on the AB1 terminal blocks.

Installation of spring technology terminal blocks is quick and simple. A screwdriver is used to open the connection point so that the conductor can be inserted into the cage. As soon as the screwdriver is pulled out, spring pressure automatically makes the contact and clamps the wire in place.

CTA-ID : 2060474
Was this helpful?
What can we do to improve the information ?