Technical FAQs

Ask a Question

What are the part #s of 18 `` and 14`` dead front trims only for NQ panelboards ?

The 18` cover only for a 225a panel  is a  8011433005  and the cover for a 400a panel is a 8012205608 .   The 14` solid cover only is a 8012205606

CTA-ID : 2060947
Was this helpful?
What can we do to improve the information ?