Technical FAQs

Ask a Question

What is the difference between the QC816F200SL, QC816F200C and QC816F200CH?

Product Features

Product Line:

Clarifying product features differences

The QC816F200_ with the ``C & CH` suffix are identical, except the ``CH`` suffix has Horn Bypass on the meter socket.
The QC816F200SL has a lever bypass meter socket and has a larger enclosure.  
NOTE: See the individual CAD drawings for each catalog number and verify Utility requirements before obtaining device

CTA-ID : 2060866
Was this helpful?
What can we do to improve the information ?