Technical FAQs

Ask a Question

What is the wire range for a NQALV1 Aluminum compression lug?

Issue:
What is the wire range for the NQALV1 aluminum compression lug?

Product Line:
NQ panelboard and accessories.

Environment:
Product specifications

Cause:
Wire Rang

Resolution:
The NQALV1 lug kit has lugs with a wire range for  (1) - #8 to 1/0 AWG. 


CTA-ID : 2060301
Was this helpful?
What can we do to improve the information ?