Technical FAQs

Ask a Question

Is there a separate incoming main lug for the neutral of a 125amp 3 phase 4 wire NF panel?

Issue:
Is there a separate incoming main lug for the neutral of a 125amp 3 phase 4 wire NF panel?

Product Line:
NF panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No, there is not.  On the 125 amp NF panel, the incoming neutral conductor is terminated at the branch neutral bar. The branch neutral bars have termination ports that will accept up to a #2/0 cable.


Revised 4/29/04


CTA-ID : 2025892
Was this helpful?
What can we do to improve the information ?