Technical FAQs

Ask a Question

QO48M30DFGPW1 and Receptacle

What type of receptacle is provided for generator hook-up to the QO48M30DFGPW1 Generator Panel?

Product Line:
PTFDS FD Enclosure Systems

QO load centers and accessories sold and supported in the USA.

Type of receptacle that is used for a generator hookup to the QO48M30DFGPW1 generator panel.

A NEMA L1430 Power Inlet is provided. The Pre-wired generator panel is OBSOLETE and NO LONGER AVAILABLE.

CTA-ID : 2060617
Was this helpful?
What can we do to improve the information ?