Technical FAQs

Ask a Question

What are the repair parts for a QO816L100DSCU, Series G2, Load Center?

Previous Design repair parts

Product Line:
QO load centers

Repair parts



Only the parts listed below are considered field replaceable.
Cover - 4055345351
Interior Assembly - 4055325050
Neutral Bonding Screw - 4028329750 Obsolete NLA. (Replaced by 40283-297-51)
Indoor Cover Mounting Screw - 4020513002K
Indoor Cover Door Hinge - 4028356450K
Door Latch Kit - 4020284450K
NOTE: Labeling is not supplied on the replacement cover and the cost of the replacement cover may be close to, or exceed, the cost of a new device. You may want to consider buying a new device and use the new cover on the existing device.

CTA-ID : 2060671
Was this helpful?
What can we do to improve the information ?