Technical FAQs

Ask a Question

What Main Circuit Breaker is used in the EZM11600GCBC and the EZM31600GCBC 1600A EZM Main Circuit Breaker?

Issue:
Product Design

Product Line:
EZM

Cause:
Clarifying main breaker provided

Resolution:
The main circuit breaker provided in both of these units is catalog number RGF36160U31A. Only the two outside phases of the breaker are used in the EZM11600GCBC. 


CTA-ID : 2060621
Was this helpful?
What can we do to improve the information ?