Technical FAQs

Ask a Question

Input voltage range for APC Silcon UPS units

The input voltage range is +/- 15% of the nominal input voltage. The tolerance for switching the unit to bypass operation is typically +/- 10%. However, this setting can be changed to +/- 4,6, or 8%.
Was this helpful?
What can we do to improve the information ?