Technical FAQs

Ask a Question

What is the recommended potentiometer size for an ATV312 drive?

Issue:
What is the recommended potentiometer size for an ATV312 drive?

Product Line:
Altivar ATV312

Environment:
All

Cause:
Needs to know what size pot they can wire up to the ATV312 drive.

Resolution:
The recommended POT size is 2.2K to 10K ohms.


CTA-ID : 2056685

Was this helpful?
What can we do to improve the information ?