Technical FAQs

Ask a Question

Do you offer the housing for the 9036DW31C in stainless steel?

No the housing is only available as standard is cast aluminum.  Older versions may be cast iron.  The two surfaces are machined to a fine tolerance, gasketed for a watertight seal.  The wetted material, however, can be stainless steel, the 9049A6CS or 9049A6S.




CTA-ID : 2060362
Was this helpful?
What can we do to improve the information ?