Technical FAQs

Ask a Question

On a NW breaker is there an option to get the bus material made out of tin plated copper rather than silver plated?

No, only silver plated copper bus is available.



CTA-ID : 2060551
Was this helpful?
What can we do to improve the information ?