Technical FAQs

Ask a Question

Does the ATV312 cooling fan run all the time?

No. The fan starts automatically when the drive controller is commanded to run (receives a run command and a speed reference). It stops a few seconds
after the drive controller is stopped (when output frequency is less than 0.5 Hz and DC injection braking is completed). Not all units have a cooling fan.
NOTE: The fan may start without a run command if the drive controller temperature exceeds allowable limits.


CTA-ID : 2058046
Was this helpful?
What can we do to improve the information ?