Technical FAQs

Ask a Question

What is a good source of information for the ATV312 drive?

Most information can be found in the following documents:
DIA2ED2090404EN is the catalog.
BBV46391 is the installation manual.
BBV46385 is the programming manual.

These documents, as well as other related literature, are available for download from http://www.schneider-electric.us or http://www.schneider-electric.com.

Reviewed 5/2011


CTA-ID : 2057568
Was this helpful?
What can we do to improve the information ?