Technical FAQs

Ask a Question

What is the difference between an XCKJ20541H7 and XCKJ10541H7?

The XCKJ10541H7 is SPDT with, with positive opening contacts, 1 normally open and 1 normally closed contact and the XCKJ20541H7  is 2 SPDT with 2 normally open and 2 normally closed contacts but does not have positive opening contacts..

CTA-ID : 2060569
Was this helpful?
What can we do to improve the information ?