Technical FAQs

Ask a Question

What is the heat dissipation for an ATS01N285LY?

23 Watts at full load at the end of starting.
514 Watts during starting and stopping at 3 times the rated operating current.


CTA-ID : 2058424
Was this helpful?
What can we do to improve the information ?