Technical FAQs

Ask a Question

What is the heat dissipation for an ATS01N230LY?

22 Watts at full load at the end of starting.
184 Watts during starting and stopping at 3 times the rated operating current.


CTA-ID : 2058422
Was this helpful?
What can we do to improve the information ?