Technical FAQs

Ask a Question

What is the replacement cover for the 9013 Type F Pressure Switch?

Issue:
What is the replacment cover for the 9013 type F pressure switch?

Product Line:
Pressure Switches

Environment:
Class 9013 type F pressure switches

Cause:
Replacement cover needed for the 9013 type F pressure switches.
 
Resolution: 

Always include the complete part number with forms, when ordering a replacement cover.

65076-792-56 is 9013 FHG Form M1 cover
65076-792-54 is 9013 FRG cover, Standard,
65076-792-55 is 9013 FRG with Form M3, M5, M1
65076-792-50 is 9013 FHG Standard or Form X.
65076-792-50  is 9013 FYG cover, standard

This part number includes the cover and the cap screw.

Others
Note: 65076-605-57 is the form Z22 black cover


 
Was this helpful?
What can we do to improve the information ?