Technical FAQs

Ask a Question

What are the repair parts for a HOM12L125RB, Series S03 load center?

Current design repair parts

Product Line:
Homeline load centers

Repair parts


Only the parts listed below are considered field replaceable.
Cover - 4056317850 (Includes hinges attached to left side of cover)
Cover Mounting Screw - 2142217101 (2 Required)
Cover Latch - 4056314701, Latch Rivet - 2410212160 (Attached to right side wall of enclosure)
Interior Trim - 4056312701 - NO LABELS
Interior Trim Mounting Screw - 4020513001K
Interior Assembly - 4056507351
Main Lugs Kit - QOL125
Neutral Bonding Screw - 4028345850K
Note: Covers and Interior Trims do not have labels applied.

CTA-ID : 2055726
Was this helpful?
What can we do to improve the information ?