Technical FAQs

Ask a Question

What are the dimensions of the fixed padlock attachments S29371 and S37422 fixed padlock attachment kits for H and J frame powerpact breakers?

It is 1.535 +/- .015 wide and 2.362 +/- .015 tall.

Composite of drawings 48035-110-01-02 and 48035-109-01-02


CTA-ID : 2060516
Was this helpful?
What can we do to improve the information ?