Technical FAQs

Ask a Question

What is the Interrupting Rating for a FJ Type Breaker?

The interrupting ratings for the FJ 2 or 3 pole breaker, 15-100A is 100K at 240V and 65K at 480V.


CTA-ID : 2060356
Was this helpful?
What can we do to improve the information ?