Technical FAQs

Ask a Question

What are the part numbers for the loose shipped hardware (contained in a cloth bag) that comes with the PFA100G enclosure?

The PFA100G should come with the following hardware contained in a cloth bag:
(3) 45102-825-01 / Line Side Breaker connector mounting screws
(2) 21916-17721 / Breaker mounting screws



CTA-ID : 2060432
Was this helpful?
What can we do to improve the information ?