Technical FAQs

Ask a Question

Does suffix MR on an SE breaker imply that it is electrically operated and includes a shunt trip and shunt close coil?

MR means they have a 120Vac spring charging motor installed.  If you need them electrically operated, then field install a shunt trip and shunt close from the offering in the latest Supplemental Digest.  As these parts are obsolete, check for availability before promising them to a customer.


CTA-ID : 2060371
Was this helpful?
What can we do to improve the information ?