Technical FAQs

Ask a Question

What is the maximum size branch breaker that can be installed in an NF panel with a 400a main breaker?

Up to two 250a K Frame sub/feed/breakers can be mounted with the proper size back box and trim ; factory installed only. The standard branch breakers go to 125a in 2 & 3 pole configuration.

Revised 6/1/04

CTA-ID : 2022222
Was this helpful?
What can we do to improve the information ?