Technical FAQs

Ask a Question

Will a 225A LA circuit breaker be series rated at 22K with a 225 A MLO NQOD panel with QO-VH circuit breakers?

No.  A 225 A LA circuit breaker will not be series rated at 22K with an NQOD MLO interior.  This is a fully rated combination.   Series ratings can be found in the Digest


CTA-ID : 2023066
Was this helpful?
What can we do to improve the information ?