Technical FAQs

Ask a Question

What is the NEMA 1 replacement enclosure only for the 8736SBG4V02S Reversing Starter?

We offer the 9991SCG9,  NEMA 1 enclosure.  

For horizontally arranged Class 8702  contactors and starters replace the reset assembly with a Class 9001 Type K51 closing plate.

CTA-ID : 2060319
Was this helpful?
What can we do to improve the information ?