Technical FAQs

Ask a Question

What is the contact rating for the MDSAN11 and MDSAN20 auxiliary contact modules

Issue:
What is the contact rating for the MDSAN11 and MDSAN20 auxiliary contact modules
 
Product Line:
Disconnect Switches - GIC Product
 
Environment:
US Product
 
Cause:
Product Specification
 
Resolution:
These auxiliary contacts are rated NEMA/UL as A600 and N600
Was this helpful?
What can we do to improve the information ?