Technical FAQs

Ask a Question

Can you order the internal components of the MD3304X MD Motor Disconnect separately?

Replacement components for the MD3304X are not available. The only accessory parts available are as follows:
MDS30P Add on power pole.
MDSAN20 Auxiliary contacts (2) normally open.
MDSAN11 Auxiliary contacts (1) normally and (1) normally closed .


CTA-ID : 2059776
Was this helpful?
What can we do to improve the information ?