Technical FAQs

Ask a Question

What is the Nema rating of the 9001KX operators?

Issue:
What is the degree of protection of the 9001KX operators? 

Product Line:
9001KX pushbuttons - GIC Product

Environment:
US Product

Cause:
Application Assistance

Resolution:
The KX operators are rated Types 1, 2, 3, 3R, 4, 12 and 13, as well as IP66

 
Was this helpful?
What can we do to improve the information ?