Technical FAQs

Ask a Question

What is a QOE250GFINM?

Cause:
Product design features

Product Line:
QO load centers

Environment:
Product description

Resolution:

The QOE250GFINM consists of a QO250GFI Ground Fault Circuit Interruptor installed in a QO2-4L60NRNM non-metallic enclosure.


CTA-ID : 2060207
Was this helpful?
What can we do to improve the information ?