Technical FAQs

Ask a Question

What is the catalog number for a field installable 120 volt shunt trip for a circuit breaker NA361200?

The NA11021 shunt trip, along with the NA361200 circuit breaker are now OBSOLETE. Consider using the P frame Powerpact breaker as a substitute; however, dimensionally, they are differerent.


CTA-ID : 2060182


Was this helpful?
What can we do to improve the information ?