Technical FAQs

Ask a Question

Is the Powerpact MG and MJ breaker 80 or 100% rated?

iT IS 80% rated. There is no option for 100% rating on this breaker.


CTA-ID : 2060079
Was this helpful?
What can we do to improve the information ?